SD.LOGEN

Description

This parameter turns on logging to the SD card.

Example

Usage

This parameter is meant to be used as part of drive NV parameters to always log to the SD card. By default, the drive creates log messages stored in the flash. In addition, if it is desired, the user can also store these log messages to the SD card. Log files are automatically rolled over when they reach 1M in size, and they are stored on the SD card, at /akd2g_drives/<drive-name>/log_files.

Code

-->DRV.HELP SD.LOGEN

Help for: SD.LOGEN [Integer] [NV] [ReadWrite]

Minval = 0

Maxval = 1

Default = 0

Actual value = 0

Extended timeout = 10 [s]

-->SD.LOGEN 1

-->SD.LOGEN 0

Versions

Action Version Notes
Implemented 02-04-01-000  

General Information

Type

Read/Write

Units

N/A

Range

0, 1
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
SD.LOGEN

3010h

01h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

SD.LOGEN

3400

D48

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

SD.LOGEN

3400

Unsigned8

Read/Write

-